Conext AGS: Solar Power System Automatic Generator Start

Automatically start and stop a generator to meet power needs

The ConextTM Automatic Generator Start (AGS) can automatically activate or stop a generator in response to changing power requirements. An excellent addition to an off-grid or backup power system, the AGS seamlessly connects to the XanbusTM network and shares status information with all other devices on the network. It can monitor a set of system user-programmable parameters such as battery voltage, state of charge or grid power and can activate the generator in response to any changes. The AGS can also be configured remotely using the Conext System Control Panel (SCP) or Conext ComBox to engage a generator, and can assist an inverter/charger when output power demands are high.

NEW! Firmware available: visit the “Download” section below.
Conext AGS Firmware V3.01 BN0001

Overview

Why choose Conext Automatic Generator Start

Higher return on investment

• Integrate with an inverter/charger to maximize system power performance

Designed for reliability

• Tested and qualified for harsh environmental conditions (HALT reliability testing)

Flexible

• Works with multiple Xanbus devices – Conext XW, SW, MPPT 60-150, MPPT 80-600, SCP, ComBox
• User-programmable trigger settings to meet specific application needs
– Battery voltage
– Exercise time
– Inverter / charger AC power loads
– SOC
– Quiet time
• Supports manual start and stop operation modes

Easy to service

• Access and troubleshoot AGS device events using the Conext ComBox or SCP
• Easily upgrade new firmware to the AGS using the ComBox

Easy to install

• Wall mount
• RJ45 connections for Xanbus network cables

Solutions

Downloads

Compatible products