Benefits

INSTALLATION FLEXIBILITY

  • Modular: includes only the components required for the application
  • Arrives pre-assembled, tested and ready, if required
  • Includes configuration toolkit for simplified installation and commissioning
  • Design verified through emulator, provides superior reliability with tested functionality

FAST ROI

  • Fuel savings and GHG reduction
  • Revenue from energy sales to the grid
  • Competitive pricing, modular design

Solutions

Schneider Electric PV Hybrid solution through partnership with DEIF includes:
  • Schneider Electric’s Conext™ CL inverter
  • DEIF’s Automatic Sustainable Controllers (ASC)
  • Automatic Genset Controllers
Schneider Electric’s Conext™ CL inverters together with DEIF’s Automatic Sustainable Controllers (ASC) and Automatic Genset Controllers provide superior coordination to deliver the highest amount of PV power for hybrid PV diesel applications. This solution works with the grid and a diesel generator to form a complete grid management solution. Conext™ CL inverters are designed to respond rapidly to power curtailment commands from controllers enabling integration of PV power in hybrid grids. The ASC from DEIF controls PV power from the Conext™ CL inverters to integrate seamlessly with diesel generator powered loads. We offer a customization option to add an Automatic Generator Controller to provide a complete plant management solution.

Off-grid application with solar power control

Grid-tied application with solar power control

Grid-tied system with complete power management

Products