Product FAQ: Which products are compatible with Conext Gateway and ComBox?

« All blog posts

Posted on: | Posted in: Product Updates, .

We want to answer one of the popular questions we are asked by our customers: which products are compatible with ConextTM Gateway and ComBox? Here is the product compatibility matrix.

 

ConextTM Gateway is compatible with our XW Pro (UL model only), XW+, SW hybrid inverter chargers as well as CL-60 and CL36 string inverters (IEC models only). Meanwhile, ConextTM ComBox is only compatible with XW+ and SW inverters.

Always please do refer to the latest datasheet for more information!

 

You can also download the Gateway and Combox Compatibility Matrix in PDF.


About the Author: Junco Kumon