Grid tie Decentralized

Commercial Grid tie Decentralized

Commercial Grid tie Decentralized TL

Commercial_grid-tie_decentralisedUsing the Conext TL, a three phase string inverter, in a commercial rooftop architecture can offer customers faster installation, lower maintenance cost and minimal system downtime.

In a decentralized set up, the PV Array is broken up into smaller sub-arrays, each with its own string inverter. When inverters are installed closer to the arrays, the cost to run DC cables are decreased. Multiple string inverters are connected to AC distribution box before to the low voltage grid. The optimized approach of three phase string inverters’ standard building block design can allow customers to scale project sizes up or down with ease.

 

commercial-pv-decentralised-tl