What to Look for in an Off-grid Solar Inverter
Mar. 24, 2014

The modern solar industry was born through off-grid solar, a market which continues to be an important aspect of the industry. Around the world, one in six people live beyond the reach of utility power, but they can rely on off-grid solar systems for electricity. In North America, off-grid solar is especially popular for buildings in remote locations where the utility grid does not yet reach, or in places prone to storms and power outages.

Off-grid solar installations are less common than grid-tie systems for a number of reasons. An off-grid system requires more components like batteries and charge controllers. With additional components, the installation is more complex and requires a higher level of technical training. It is also more costly for the end user, and not all end users need off-grid solar.
Although off-grid is more complex than grid-tie, the off-grid market continues to grow and there is a shift with experienced installers beginning to move from the competitive grid-tie market to the more lucrative off-grid market. Solar product suppliers are also working to make off-grid installations easier. Look for the following offers:

Off-Grid Packages

blog-post-img1

Off-grid system integrators can lessen the complexity of an off-grid
system by providing easy-to-install packages. A package can include an inverter/charger, solar
charge controllers, control panels and accessories. The components should all work together upon
taking them out of the box. Ordering an off-grid system as a package also ensures all the necessary
parts are together and eliminating the need to contact the supplier from a job site to rush a
forgotten part.

Flexible Off-Grid Inverters

Another way to cut down on the
complexity of off-grid solar projects is to find an inverter/charger that is flexible enough to meet
any installation requirement. Look for inverters with intelligent load management to handle a
diverse set of energy loads. Load management becomes incredibly important when connecting your
inverter to a generator, or to the utility grid. Some inverters have dual AC inputs to accommodate
both the generator and the grid, which lowers the additional system component requirements and
allows more flexibility in covering differing system needs.

blog-post-img2

Connecting an off-grid solar system to
the utility grid (where possible) also gives the end user the opportunity to sell back excess energy
to their utility company.

Stackable Off-Grid Inverters

Building an off-grid solar
system requires a sizeable up-front investment. It is common for homeowners to start with a
smaller-size system, with plans to add on at a later date. Adding more solar is easy when starting
with an inverter that can be stacked together with other inverters. It is also becoming more common
to attach an off-grid solar inverter to an existing grid-tie solar system through AC coupling. A
grid-tie solar system is great, but it requires utility power to operate and shuts off during any
utility power outages. Only off-grid inverters paired with batteries will provide uninterrupted
power for critical loads.

Customer Service

As mentioned earlier, off-grid solar
systems are useful for buildings in remote locations. However, remote locations require extra travel
time to reach. To cut back on site visits, choose inverters that have proven reliability and will
last for years. Trust suppliers that have been financially successful in the off-grid market for
many years. Ask them to provide references for older installations, or show you how the product is
internally tested. If service is necessary, it’s important the supplier be available to troubleshoot
and provide quick resolution. The supplier should also be accessible by the end user for
emergencies. New technology makes troubleshooting quicker by allowing remote connections to the
off-grid inverter. This can be done through a remote monitoring system. Look for systems that can
also upgrade firmware remotely. As the off-grid solar market continues to grow, these offerings will
ensure that off-grid off-grid solar installations are safe, reliable, and cost effective.

By:
Ray Barbee, director of channel development; Stephanie Byrd, marketing communications specialist, US
Solar,Schneider Electric